To implement a method call, the actual parameters (arguments) are passed to the interface variables. As an alternative, the parameter names can be omitted.
Depending on the declared access specifier, a method can be called only within its
own namespace (INTERNAL), only within its own POU and its derivatives (PROTECTED), or only within its own POU (PRIVATE). For PUBLIC, the method can be called from anywhere.
Within the implementation, a method can recursively call itself, either directly by
means of the THIS pointer, or by means of a local variable for the assigned function block.
-
Method call as a virtual function call
-
Example
-
Additional outputs
-
Calling a method even if the application is in the STOP state
-
Calling methods recursively